contact us

Contact Haas

Haas Europe Headquarters: BelgiumMercuriusstraat 28 B-1930 Zaventem, Belgium
Phone: +32 2-522-99 05
Europe@haascnc.com Find A Distributor
Questions & Comments

Looking for the Haas USA site?

 
International
Haas Automation Inc

Haas CNC Control

Years of development have gone into designing the best control hardware and software in the industry. Our new generation machines pack even more innovation into what was already the industry's greatest overall CNC control. To ensure smooth, precise motion control, Haas machine tools use next-generation digital servomotors and high-resolution encoders on all axes. These combine with significant software and motor-control advancements to yield better surface-finish performance than ever before.

 

About The Haas CNC Control

 

print

Closed System

Our focus is to provide a robust, dependable control that is seamlessly integrated with the machine. Our closed system is optimized specifically for Haas machines, and does not rely on third-party NC suppliers. When you call Haas, you get a company that takes full responsibility for the entire machine.

Dedicated Keypad

The Haas keypad has a full array of keys, including a complete alphanumeric keypad, and all common functions are clearly labeled for operator ease. If you've ever fumbled with hot keys, or had to page through screens looking for a specific function, you will appreciate the simplicity of the Haas control. There are no encrypted codes to memorize.

One-Button Features

Common multi-step functions, such as setting tool offsets, have been reduced to the push of a single button. Other often-used functions, such as setting work offsets, homing the machine, and selecting the next tool during setup, are also one-button commands.

Multi-Function Jog Handle

Most machines use the jog handle only to move the axis around. On Haas machines, the jog handle can also be used in other modes to cursor through the program for faster editing, override spindle speeds and feedrates, or scan through offsets, parameters, etc.

15" Color LCD Screen

Our full-color, 15" TFT LCD display is designed to work in the machine shop environment. The high-density, high-contrast LCD features a very wide viewing angle, and will not wash out in bright light. The panel is mounted behind anti-glare, tempered glass for protection and easy viewing.

USB Port

The built-in USB port allows the use of customer-supplied USB flash memory devices or external hard drives.

go to top

CNC Control for Haas VMC/HMC Mills

 

print

Standard Features

  • Tool/work offsets:
    • one-button inputs
    • cutter compensation (radius/dia.)
    • 200 geometry/wear offsets
    • 105 work offsets
  • 1 MB program memory
  • Triple 32-bit processors
  • ISO standard G-code compatibility
  • Tool life management
  • Tool load monitoring
  • Helical interpolation
  • Background editing
  • Split screen program review
  • Trig calculator
  • Speeds and feeds calculator
  • Arc calculator
  • Inch or metric programming
  • USB port
  • RS-232 port
  • DNC link
  • Mid-program restart
  • Message page
  • Selectable languages
  • Self-diagnostics
  • Fully descriptive alarms
  • Programmable mirror imaging
  • Advanced pocket milling
  • Bolt-hole drilling
  • Graphic dry run
  • Dedicated keypad
  • High-speed communication
  • S-curve acceleration
  • Multi-function jog handle
  • Engraving
  • Rigid tapping
  • Contour accuracy control
  • Memory Lock Keyswitch
  • Made in the USA
  • Worldwide service network

VF-3.jpg

Available Control Options for Haas Mills:

  • Haas Intuitive Programming System
  • High-Speed Machining
  • Memory Upgrades
  • 8 M Functions
  • User-Definable Macros
  • User-Defined Second Home Position
  • Haas Intuitive Probing System
  • 4th- & 5th-Axis Control
  • Remote Jog Handle
  • Coordinate Rotation/Scaling
  • Ethernet Interface
go to top

CNC Control for Haas Lathes

 

print

Standard Features

  • Tool/work offsets:
    • One-button inputs
    • 50 tool geometry/wear/taper offsets
    • Tool nose radius compensation
    • 105 work offsets
  • Triple 32-bit processors
  • 1 MB program memory
  • ISO standard G-code compatibility
  • Tool life management
  • Tool load monitoring
  • Helical interpolation
  • Background editing
  • Split screen program review
  • Trig calculator
  • Speeds and feeds calculator
  • Arc calculator
  • Mid-program restart
  • USB port
  • RS-232 port
  • DNC link
  • Inch or metric programming
  • Message page
  • Selectable languages
  • Self-diagnostics
  • Fully descriptive alarms
  • Programmable mirror imaging
  • Advanced pocket milling
  • Bolt-hole drilling
  • Graphic dry run
  • Dedicated keypad
  • High-speed communication
  • Multi-function jog handle
  • Engraving
  • Rigid tapping
  • Contour accuracy control
  • Memory Lock Keyswitch
  • Made in the USA

ST-20.jpg

Available Control Options for Haas Lathes:

  • Haas Intuitive Programming System
  • Memory Upgrades
  • 8 M Functions
  • User-Definable Macros
  • Work Offset Probing
  • Tool Offset Probing
  • Remote Jog Handle
  • Ethernet Interface
  • Spindle Orientation

go to top

Control Simulators

 
simulator.jpg print

Use the Haas Control Simulator for classroom training and/or on-site control demonstrations. Teach programming and operations using a real, fully upgradable Haas control panel and keypad. Includes simulated dry run graphics, tool length measurement, true DNC and USB convenience. You can also program and download directly from the Control Simulator to Haas machines.

Control Simulator Module Dual Machine
Part: CSMD
Price: $1,695.00

go to top